|
Glossary Definition for Bandwidth
Glossary Term: Bandwidth
- Definition
-
1. Bandwidth (BW) is a range of frequencies, or information, that a circuit can handle or the range of frequencies that a signal contains or occupies.
Example: An AM broadcast radio channel in the US has a bandwidth of 10kHz, meaning that it occupies a 10kHz-wide band, such as the frequencies from 760kHz to 770kHz.
2. The amount of data a digital channel or line can handle, expressed in bits per second (bps), kilobits per second (kbps), baud, or a similar measure.
Synonyms
- band
- Mbps
- megabits
- kilobits
- kbps
- bps
- BW
Find a term alphabetically:
Comment on This Term (Corrections, Suggestions, etc.)
Suggest Another Term We Should Add
|