Maxim at a Glance
At Maxim, we invent highly integrated solutions that make technology seamless. We channel our collective expertise to stretch the limits of technology, understand your needs, and help you get to market faster.
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
Keywords: battery charger, buck-mode switching regulator, synchronous rectifier, charge pump, charging efficiency Related Parts
APPLICATION NOTE 851
Battery Charger Delivers 2.5A with > 96% Efficiency
Oct 12, 1995
Abstract: This design note shows how a circuit with modified feedback paths transforms a switch-mode power supply into a highly efficient battery charger. The battery charger is based on a step-down controller, the MAX797, and charges up to six cells with > 96% efficiency at higher output voltages.
A related idea appeared in the October 12, 1995 issue of EDN.
Battery chargers are usually designed without regard for efficiency, but the heat generated by low-efficiency chargers can present a problem. For those applications, the charger of Figure 1 delivers 2.5A with efficiency as high as 96%. It can charge a battery of one to six cells while operating from a car battery.
Figure 1. Modified feedback paths transform this switchmode power-supply circuit for notebook computers into a high-efficiency battery charger.
IC1 is a buck-mode switching regulator that controls the external power switch, Q1, and the synchronous rectifier, Q2. These n-channel MOSFETs are more efficient than equivalent p-channel types because their on-resistance is lower; therefore they drop less voltage when conducting a given amount of current. IC1 includes a charge pump for generating the positive gate-drive voltage required by Q1.
The battery-charging current develops a voltage across the 25mΩ resistor R3 that is amplified by the op amp and presented as positive-voltage feedback to IC1. This feedback enables the chip to maintain the charging current at 2.5A. While charging, the circuit can also supply current to a separate load, up to a limit set by the current-sense transformer, T1, and sense resistor, R1.
T1 improves efficiency by lowering power dissipation in R1. The transformer turns ratio (1:70) routes only 1/70 of the total battery-plus-load current through R1, creating a feedback voltage that enables IC1 to limit the overall current to a level compatible with the external components.
Efficiency exceeds 96% at the higher output voltages (Figure 2). (Lower output voltage produces less output power, so the relatively fixed amount of dissipation associated with Q1, Q2, and IC1 represents a larger percentage of the total.) If you inadvertently disconnect the battery during a charge, VOUT cannot rise to a dangerous level (as it can in a boost-mode topology) because the charger's buck-mode topology limits the maximum output voltage to VIN.
Figure 2. Efficiency for the Figure 1 battery charger rises with output voltage.