Maxim at a Glance
At Maxim, we invent highly integrated solutions that make technology seamless. We channel our collective expertise to stretch the limits of technology, understand your needs, and help you get to market faster.
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
Keywords: RTC, example, software, super capacitor, real time clock, trickle charger, super cap Related Parts
APPLICATION NOTE 511
Using the DS1672 Low-Voltage Serial Timekeeping IC
Aug 27, 2002
Abstract: This application note provides an example schematic and software for the DS1672. The example software converts the 32-bit elapsed time value in the real-time clock (RTC) to year, month, date and time format. The example uses a super capacitor (super cap) to maintain the time and date when main power is absent.
Pin Assignment (Top View)
Description
The DS1672 is a low-voltage serial timekeeping
IC. The DS1672 counts seconds in a 32-bit
register. Using a 32-bit binary register instead of
a BCD representation of the time and date, as
many real-time clocks do, can be useful where
time intervals are to be measured. The DS1672
operates from a low-voltage supply (2.0V, 3.0V,
or 3.3V) and includes a VBACKUP input, which
allows the DS1672 to continue running the
counter from a backup supply, such as a battery,
while the main supply is off.
The DS1672 also incorporates a trickle charger. The trickle charger register uses four bits to enable the
charger. Two bits are used to select one of three current- limiting resistors and two bits to select one or
zero series diodes. The trickle charger circuit is capable of charging a rechargeable battery or a large
capacitor. The VBACKUP pin can also be connected to a nonrechargeable battery, such as a lithium coincell.
In that case, the trickle charger should not be enabled.
In this example, the DS1672 is configured to charge a capacitor connected to VBACKUP.
A schematic of the circuit is shown in Figure 1. Figure 2 shows the discharge voltage versus
time in a typical application. Software for initializing the DS1672 and reading the registers is shown in
Figure 3.
Figure 2. DS1672-3 VBACKUP Timekeeping Operation with 0.1F Backup Capacitor.
Figure 3. DS1672 Initialization Software
/***************************************************************************/
/* DS1672AN.C - This file is provided to show an example of communication */
/* routines for interfacing to the DS1672. These routines are provided */
/* for example only and are not supported by Dallas Semiconductor/Maxim */
/***************************************************************************/
#include <stdio.h> /* Prototypes for I/O functions */
#include <DS5000.h> /* Register declarations for DS5000 */
#define ACK 0
#define NACK 1
#define ADDRTC 0xd0 /* 2-wire addresses */
sbit scl = P1^0; /* 2-wire pin definitions */
sbit sda = P1^1;
sbit RSTb = P0^2;
void start2w();
void stop2w();
void writebyte2w(uchar d);
uchar readbyte2w(int);
void writebyte1672();
void initialize_DS1672();
void disp_clk_regs();
void en_tc();
unsigned long date2day(uint, uint, uint, uint, uint, uint);
void day2date(unsigned long);
/* global variables */
void start2w() /* --------- Initiate start condition ---------- */
{
sda = 1; scl = 1;
sda = 0;
}
void stop2w() /* ---------- Initiate stop condition ----------- */
{
sda = 0; sda = 0;
scl = 1; scl = 1; sda = 1;
}
void writebyte2w(uchar d) /* ----------------------------- */
{
int i;
scl = 0;
for (i = 0;i < 8; i++)
{
if (d & 0x80)
sda = 1; /* Send the msbits first */
else
sda = 0;
scl = 0;
scl = 1;
d = d << 1; /* do shift here to increase scl high time */
scl = 0;
}
sda = 1; /* Release the sda line */
scl = 0;
scl = 1;
if (sda) printf("Ack bit missing %02X\n",(unsigned int)d);
scl = 0;
}
uchar readbyte2w(int b) /* ----------------------------------- */
{
int i;
uchar d;
d = 0;
sda = 1; /* Let go of sda line */
scl = 0;
for (i = 0; i < 8; i++) /* read the msb first */
{
scl = 1;
d = d << 1;
d = d | (unsigned char)sda;
scl = 0;
}
sda = b; /* low for ack, high for nack */
scl = 1;
scl = 0;
sda = 1; /* Release the sda line */
return d;
}
void day2date(unsigned long x) /* ------ convert binary time to date format ---
--- */
{
int yrs = 99, mon = 99, day = 99, tmp, jday, hrs, min, sec;
unsigned long j, n;
j = x / 60; /* whole minutes since 1/1/70 */
sec = x - (60 * j); /* leftover seconds */
n = j / 60;
min = j - (60 * n);
j = n / 24;
hrs = n - (24 * j);
j = j + (365 + 366); /* whole days since 1/1/68 */
day = j / ((4 * 365) + 1);
tmp = j % ((4 * 365) + 1);
if(tmp >= (31 + 29)) /* if past 2/29 */
day++; /* add a leap day */
yrs = (j - day) / 365; /* whole years since 1968 */
jday = j - (yrs * 365) - day; /* days since 1/1 of current year */
if(tmp <= 365 && tmp >= 60) /* if past 2/29 and a leap year then */
jday++; /* add a leap day */
yrs += 1968; /* calculate year */
for(mon = 12; mon > 0; mon--)
{
switch(mon)
{
case 1: tmp = 0; break;
case 2: tmp = 31; break;
case 3: tmp = 59; break;
case 4: tmp = 90; break;
case 5: tmp = 120; break;
case 6: tmp = 151; break;
case 7: tmp = 181; break;
case 8: tmp = 212; break;
case 9: tmp = 243; break;
case 10: tmp = 273; break;
case 11: tmp = 304; break;
case 12: tmp = 334; break;
}
if((mon > 2) && !(yrs % 4)) /* adjust for leap year */
tmp++;
if(jday >= tmp) break;
}
day = jday - tmp + 1; /* calculate day in month */
printf("\n%04d %02d %02d %02d:%02d:%02d", yrs ,mon, day, hrs, min, sec);
}
/* ---- convert date to elapsed days in binary ---- */
unsigned long date2day(uint yr, uint mo, uint da, uint hrs, uint min, uint sec)
{
unsigned long x;
/* the following is broken down for clarity */
x = 365 * (yr - 1970); /* calculate number of days for previous
years */
x += (yr - 1969) >> 2; /* add a day for each leap year */
if((mo > 2) && (yr % 4 == 0)) /* add a day if current year is leap and
past Feb 29th */
x++;
switch(mo)
{
case 1: x += 0; break;
case 2: x += 31; break;
case 3: x += 59; break;
case 4: x += 90; break;
case 5: x += 120; break;
case 6: x += 151; break;
case 7: x += 181; break;
case 8: x += 212; break;
case 9: x += 243; break;
case 10: x += 273; break;
case 11: x += 304; break;
case 12: x += 334; break;
}
x += da - 1; /* finally, add the days into the
current month */
x = x * 86400; /* and calculate the number of seconds in
all those days */
x += (hrs * 1800); /* add the number of seconds in the hours
*/
x += (hrs * 1800); /* add the number of seconds in the hours
*/
x += (min * 60); /* ditto the minutes */
x += sec; /* finally, the seconds */
return(x);
}
void writebyte1672() /* ----------------------------------------------- */
{
uchar Add;
uchar Data;
/* Get Address & Data */
printf("\nEnter the Read Address\nADDRESS:");
scanf("%bx", &Add);
printf("\nDATA:");
scanf("%bx", &Data);
start2w();
writebyte2w(ADDRTC);
writebyte2w(Add);
writebyte2w(Data);
stop2w();
}
void initialize_DS1672() /* ----------------------------------------- */
/* Note: NO error checking is done on the user entries! */
{
uchar a, b, c, d;
uint yr, mn, dt, dy, hr, min, sec, day;
unsigned long y;
start2w();
writebyte2w(ADDRTC);
writebyte2w(0x04);
writebyte2w(0x00); /* enable the oscillator */
stop2w();
printf("\nEnter the year (1970-2099): ");
scanf("%d", &yr);
printf("\nEnter the month (1-12): ");
scanf("%d", &mn);
printf("\nEnter the date (1-31): ");
scanf("%d", &dt);
/* printf("\nEnter the day (1-7): "); */
/* scanf("%d", &dy); */
printf("\nEnter the hour (1-24): ");
scanf("%d", &hr);
printf("\nEnter the minute (0-59): ");
scanf("%d", &min);
printf("\nEnter the second (0-59): ");
scanf("%d", &sec);
y = date2day(yr, mn, dt, hr, min, sec);
a = (y & 0xff);
b = ((y >> 8) & 0xff);
c = ((y >> 16) & 0xff);
d = ((y >> 24) & 0xff);
start2w();
writebyte2w(ADDRTC); /* write slave address, write 1672 */
writebyte2w(0x00); /* write register address, 1st clock register */
writebyte2w(a);
writebyte2w(b);
writebyte2w(c);
writebyte2w(d);
stop2w();
}
void disp_clk_regs() /* ----------------------------------------- */
{
uchar reg1, prv_sec = 99, reg2, reg3, reg4;
unsigned long z;
while(!RI) /* Read & Display Clock Registers */
start2w();
writebyte2w(ADDRTC); /* write slave address, write 1672 */
writebyte2w(0x00); /* write register address, 1st clock register */
start2w();
writebyte2w(ADDRTC | 1); /* write slave address, read 1672 */
reg1 = readbyte2w(ACK); /* starts w/last address stored in register pointer */
reg2 = readbyte2w(ACK);
reg3 = readbyte2w(ACK);
reg4 = readbyte2w(NACK);
stop2w();
if(reg1 != prv_sec) /* display every time seconds change */
{
z = reg4;
z <<= 8;
z += reg3;
z <<= 8;
z += reg2;
z <<= 8;
z += reg1;
day2date(z);
}
prv_sec = reg1;
}
RI = 0; /* Swallow keypress to exit loop */
}
void en_tc(dat) /* ----- enable the trickle-charger ------ */
{
start2w();
writebyte2w(ADDRTC);
writebyte2w(5);
writebyte2w(dat); /* enable the trickle-charger */
stop2w();
}
main (void) /* ----------------------------------------------------- */
{
uchar i, M, M1;
RSTb = 1;
while (1)
{
printf("\nDS1672\n");
printf("I Init DS1672 D/E Disable/Enable TC\n");
printf("R Read Time W Write Byte\n");
printf("\nEnter Menu Selection:");
M = _getkey();
switch(M)
{
case 'R':
case 'r': disp_clk_regs(); break;
case 'W':
case 'w': writebyte1672(); break;
case 'D':
case 'd': en_tc(0); break;
case 'E':
case 'e': en_tc(0xa6); break;
case 'I':
case 'i': initialize_DS1672(); break;
}
}
}