TUTORIAL 4678

Advantages of Internet Protocol (IP) Cameras and H.264 Compression for Security and Surveillance Video

By:  Piero Bianco, Business Manager, SPM Business Unit
May 10, 2010

Abstract: This application note discusses the advantages Internet protocol (IP) cameras have in security and surveillance video systems over analog cameras. Unlike their predecessors, IP cameras support high-definition (HD) images, local data storage, video analytics, and remote control functionality. The application note also details the benefits of using H.264 video compression technology for IP camera networks, and presents Maxim's Mobicam3 IP camera reference design kit.

Attend this brief webcast by Maxim on TechOnline
Attend this brief webcast by Maxim on TechOnline

Overview

IP cameras use the Internet protocol (IP) to transmit audio and video data, along with control signals, over Ethernet links in closed-circuit television (CCTV) systems. They offer numerous advantages over traditional analog security cameras, which typically transmit an analog NTSC/PAL signal over coaxial cable. Unlike analog cameras, IP cameras support high-definition (HD) images, intelligent analytics, local video storage, and remote control.

Video compression is performed in the IP camera together with analytic functions, video encryption (to stop hackers), and encapsulation of video data into Ethernet packets. The compressed video stream is usually sent to a hybrid digital video recorder (DVR) or network video recorder (NVR) for storage, playback, and display. The use of an IP network for video monitoring can enable security staff to be located at geographically remote locations, allowing centralized control over security cameras across campuses or multiple sites using pan-tilt-zoom (PTZ) commands sent over the IP network.

Low-power camera designs can be powered over Ethernet (PoE) without additional power sources. By using the same cable to transmit both data and power, PoE installations can substantially reduce cabling costs. In some cases, wireless networks such as Wi-Fi® can be used to replace Ethernet, thus easing camera placement. This is especially true of home security cameras where Ethernet wiring may not be readily available, and where "cloud computing" DVR applications replace physical DVRs.

Multistream H.264 and Motion-JPEG Compression

The H.264 video compression standard provides approximately twice the compression of the previous MPEG-4 standard for the same video quality. Within the H.264 standard, the "high" profile defines the highest video quality with the lowest bit rate, making it especially relevant for applications such as video security. Achieving very-low-latency (delay) encoding minimizes the response time from security personnel. Meanwhile, high-definition video encoding enables the IP camera to capture details such as facial features and license plates for enhanced security imaging. Since network bandwidth may be limited, systems can require the ability to encode/record one HD stream over a local area network (LAN) while simultaneously streaming a lower resolution feed for remote viewing over a wide area network (WAN).

Mobicam3 720p H.264/M-JPEG IP camera reference design
Mobicam3 720p H.264/M-JPEG IP camera reference design

In addition to H.264, many security systems require backward compatibility with existing equipment that does not support H.264. The Motion-JPEG (M-JPEG) standard can provide backward compatibility in such systems, as well as the ability to take high-resolution lossless snapshots. Specifically, it supports simultaneous encoding of H.264 video for uninterrupted video recording while capturing JPEG still images, which may be driven by specific events.

Analytics

Video analytics is the process of analyzing video data and making decisions based upon it. Supporting analytics in software within the camera enables actions to be taken immediately based on specific events and without the need for inputs from security personnel. For example, an alarm may be sounded if the camera detects that a person has crossed into a secure area. Analytic functions include motion detection, trip wire, and image tracking. All of these functions need to be configurable from the PC-based security management software using an intuitive graphical user interface (GUI).

IP camera block diagram. For a list of Maxim's recommended solutions, please visit: www.maximintegrated.com/IPcamera.
IP camera block diagram. For a list of Maxim's recommended solutions, please visit: www.maximintegrated.com/IPcamera.

Embedded Linux® Software and Networking

IP cameras need to provide the capability for streaming video to multiple clients. For example, Maxim's IP camera reference design (Mobicam3) supports up to 16 clients and both the real-time transport protocol (RTP) and the real-time streaming protocol (RTSP). The following Ethernet protocols are also supported: HTTP, DHCP, SMTP, TCP/IP, UDP, TFTP, FTP, NTP, and UPnP™. Streams can be encrypted using AES or SHA encryption to prevent hacking or tampering.

Linux is a registered trademark of Linus Torvalds.

UPnP is a registered certification mark of the UPnP Forum.

Wi-Fi is a registered certification mark of Wi-Fi Alliance Corporation.



Related Parts
MAX15000 Current-Mode PWM Controllers with Programmable Switching Frequency Free Samples  
MAX15001 Current-Mode PWM Controllers with Programmable Switching Frequency Free Samples  
MAX5941 IEEE 802.3af-Compliant Power-Over-Ethernet Interface/PWM Controller for Power Devices Free Samples  
MAX5942 IEEE 802.3af Power-Over-Ethernet Interface/PWM Controller for Power Devices Free Samples  
MAX5969A IEEE 802.3af/at-Compliant, Powered Device Interface Controllers with Integrated Power MOSFET Free Samples  
MAX5969B IEEE 802.3af/at-Compliant, Powered Device Interface Controllers with Integrated Power MOSFET Free Samples  
MAX9526 Low-Power, High-Performance NTSC/PAL Video Decoder  
MAX9718 Low-Cost, Mono/Stereo, 1.4W Differential Audio Power Amplifiers Free Samples  
MAX9860 16-Bit Mono Audio Voice Codec Free Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (91.5kB)  
Share
Other Channels  Email this page to an associate or friend. 



APP 4678: May 10, 2010
TUTORIAL 4678, AN4678, AN 4678, APP4678, Appnote4678, Appnote 4678

Share



More