APPLICATION NOTE 4543

Precision Circuit Monitors Negative-Supply Thresholds

By:  Kevin Bilke, Applications Engineer
Dec 07, 2010

Abstract: Using an IC (MAX971) that includes an open-drain comparator and a precision 1% voltage reference, this circuit monitors the magnitude of a negative supply voltage and provides a digital warning of fault conditions. To monitor multiple negative voltages, use the MAX974, which includes four comparators.

A similar version of this article appeared in the February 8, 2008 issue of Portable Design magazine.

A simple but accurate circuit (Figure 1) monitors the magnitude of a negative supply voltage. This capability is useful in multi-rail systems, particularly if the negative rail serves as the precision bias voltage for a GaAs device. The IC (MAX971) includes an open-drain comparator and a precision 1% voltage reference. Its trigger threshold is set by the value of external resistor R4. For convenience, all other resistors have the value 1MΩ.

Figure 1. The output of this negative-voltage monitor goes low when the monitored negative voltage is above (more negative than) the threshold set by R4.
Figure 1. The output of this negative-voltage monitor goes low when the monitored negative voltage is above (more negative than) the threshold set by R4.

Resistors R1 and R2 divide the reference voltage, providing a trip point of Vref/2 for the comparator. R3 and R4 sample the negative voltage, and IC1 compares that sample to the trip-point voltage. R4 = 1MΩ + 2(1MΩ × VNEG/1.182V), where VNEG is the magnitude of the voltage being monitored (ignoring the minus sign). The circuit output goes low in response to a fault condition—i.e., when the magnitude of the monitored voltage drops below the set threshold. To ensure an overall accuracy better than 2%, all resistors should have 1% tolerance.

For monitoring more than one negative voltage, choose the MAX974, which includes four open-drain comparators with a precision 1% reference. Feed the output of R1 and R2 to all the comparators, add an R3/R4 pair for each monitored voltage, and calculate each R4 to yield a trip point for the corresponding voltage. All the open-drain outputs can be connected together.

Related Parts
MAX971 Ultra-Low-Power, Open-Drain, Single/Dual-Supply Comparators Free Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (57kB)  
Share
Other Channels  Email this page to an associate or friend. 



APP 4543: Dec 07, 2010
APPLICATION NOTE 4543, AN4543, AN 4543, APP4543, Appnote4543, Appnote 4543

Share



More