APPLICATION NOTE 3989

Add Control, Memory, Security, and Mixed-Signal Functions with a Single Contact

Feb 09, 2007

Abstract: This application note provides a high-level overview of the 1-Wire® interface. It discusses power and data delivery along with data-bit-level communication, device selection, and the unalterable, unique ID in each device. As its name implies, the single-contact 1-Wire interface is an unmatched solution that provides key functions to systems where interconnect must be minimized.

Overview

The Maxim 1-Wire bus is a simple signaling scheme that performs half-duplex bidirectional communications between a host/master controller and one or more slaves sharing a common data line (Figure 1). Both power and data communication for slave devices are transmitted over this single 1-Wire line. For power delivery, slaves capture charge on an internal capacitor when the line is in a high state and then use this charge for device operation when the line is low during data transmission. A typical 1-Wire master consists of an open-drain I/O port pin and a 3V to 5V resistor pullup. More sophisticated masters, including dedicated line-driver solutions, are available from Maxim. This clever communication scheme also allows you to add memory, authentication, and mixed-signal functions at any time, easily and efficiently.

Figure 1. In a 1-Wire master/slave configuration, all devices share a common data line.
Figure 1. In a 1-Wire master/slave configuration, all devices share a common data line.

64-Bit Serial Numbers

There is an important, fundamental feature in every 1-Wire system: each slave device has a unique, unalterable (ROM), 64-bit, factory-lasered serial number (ID) that will never be repeated in another device. Besides providing a unique electronic ID to the end product, this 64-bit ID value allows the master device to select a slave device among the many that can be connected to the same bus wire. Part of the 64-bit ID is also an 8-bit family code that identifies the device type and functionality supported.

Data-Bit-Level Communication

The bus master initiates and controls all 1-Wire communication. As illustrated in Figure 2, the 1-Wire communication waveform is similar to pulse-width modulation, because data is transmitted by wide (logic 0) and narrow (logic 1) pulse widths during data-bit time periods or time slots. A communication sequence starts when the bus master drives a defined length "Reset" pulse that synchronizes the entire bus. Every slave responds to the Reset pulse with a logic-low "Presence" pulse. To write data, the master first initiates a time slot by driving the 1-Wire line low, and then either holds the line low (wide pulse) to transmit a logic 0 or releases the line (short pulse) to allow the bus to return to the logic 1 state. To read data, the master again initiates a time slot by driving the line with a narrow low pulse. Slaves can then either return a logic 0 by turning on the open-drain output and holding the line low to extend the pulse, or a logic 1 by leaving the open-drain output off to allow the line to recover. Most 1-Wire devices support two data rates: Standard speed of about 15kbps and Overdrive speed of about 111kbps. The protocol is self-clocking and tolerates long inter-bit delays, which ensures smooth operation in interrupted software environments.

Figure 2. This waveform example shows master-initiated write/read of data bits with slave and master sampling points.
Figure 2. This waveform example shows master-initiated write/read of data bits with slave and master sampling points.

Device Selection

The first action in a 1-Wire communication is selecting a slave device for subsequent communications. In a single slave-device environment, the selection sequence is minimal. In a multidevice environment, however, slave selection is done either by selecting all slaves or a specific slave targeted by its 64-bit ID. A binary search algorithm (described as ROM-level commands in the 1-Wire literature) "learns" and subsequently selects the respective 64-bit IDs of all slave devices on the line. When a specific slave is selected, the master issues device-specific commands and sends data to it, or reads data from it. Meanwhile, all the other slave devices ignore communications until the next reset pulse is issued.

Summary

You can layer a variety of memory, digital, analog, and mixed-signal functions onto a 1-Wire communication system. The resulting diverse product portfolio will definitely solve interconnect limitations in a constrained design and/or add value with unique product features. The 1-Wire products are available in standard IC packaging and the Company's rugged, stainless steel iButton® package. Products, packaging, and extensive software support are detailed at: 1-Wire. For a more text-oriented presentation of 1-Wire devices, see application note 1796, "Overview of 1-Wire Technology and Its Use." Maxim's 1-Wire products have more than 15 years of history in the medical field. Application note 4702, "Easily Add Memory, Security, Monitoring, and Control to Medical Sensors and Consumables," provides details and practical examples.

1-Wire is a registered trademark of Maxim Integrated Products, Inc.

iButton is a registered trademark of Maxim Integrated Products, Inc.



Related Parts
DS2401 Silicon Serial Number Free Samples  
DS2406 Dual Addressable Switch Plus 1Kb Memory Free Samples  
DS2411 Silicon Serial Number with VCC Input Free Samples  
DS2413 1-Wire Dual Channel Addressable Switch Free Samples  
DS2417 1-Wire Time Chip With Interrupt Free Samples  
DS2431 1024-Bit 1-Wire EEPROM Free Samples  
DS2432 1Kb Protected 1-Wire EEPROM with SHA-1 Engine Free Samples  
DS2450 1-Wire Quad A/D Converter  
DS2480B Serial to 1-Wire Line Driver Free Samples  
DS2482-100 Single-Channel 1-Wire Master Free Samples  
DS2502 1Kb Add-Only Memory Free Samples  
DS2505 16Kb Add-Only Memory Free Samples  
DS28E01-100 1Kb Protected 1-Wire EEPROM with SHA-1 Engine Free Samples  
DS28E04-100 4096-Bit Addressable 1-Wire EEPROM with PIO  
DS28EA00 1-Wire Digital Thermometer with Sequence Detect and PIO Free Samples  
DS28EC20 20Kb 1-Wire EEPROM Free Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (43kB)  
Share
Other Channels  Email this page to an associate or friend. 



APP 3989: Feb 09, 2007
APPLICATION NOTE 3989, AN3989, AN 3989, APP3989, Appnote3989, Appnote 3989

Share



More