APPLICATION NOTE 3921

Using a DS1307 with a PIC Microcontroller

Sep 29, 2006

Abstract: This application note is intended to demonstrate an application using the DS1307 real-time clock (RTC) with a Microchip PIC microcontroller. The software example includes basic operating routines. A schematic of the application circuit is included.

Discussion

This application note demonstrates how to use the DS1307 real-time clock (RTC) with a Microchip PIC16F628 microcontroller.

The example code, written in assembly code, includes a routine for reading the time and date from the RTC and a routine to write time and date data to the RTC from user entries.

Operation

The program uses two general-purpose port pins on the microcontroller to communicate with the DS1307 using the I²C serial interface. The microcontroller's internal UART drives two port pins, which are connected to a DS232 line driver/receiver. User inputs and data outputs from the program are passed through the RS-232 interface from a terminal emulator program on a PC to the microcontroller. The RS-232 DTR input line controls the microcontroller's reset input.

The microcontroller in this example is a PIC16F628. For information on the microcontroller used in this application note, including available programming tools, visit the Microchip web site.

The software is shown in Figure 1. A schematic of the circuit is shown in Figure 2.

Figure 1. Program Listing
Download (TXT, 10kB)

Figure 1. Program Listing

Figure 2. Schematic drawing of the DS1307 circuit used with a PIC microcontroller.
More detailed image (PDF, 126kB)

Figure 2. Schematic drawing of the DS1307 circuit used with a PIC microcontroller.



Related Parts
DS1307 64 x 8, Serial, I²C Real-Time Clock Free Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (39kB)  
Share
Other Channels  Email this page to an associate or friend. 



APP 3921: Sep 29, 2006
APPLICATION NOTE 3921, AN3921, AN 3921, APP3921, Appnote3921, Appnote 3921

Share



More