APPLICATION NOTE 3212

Quick-Start: Driving 16-Segment Displays with the MAX6954

Jun 25, 2004

Abstract: This article is how-to guide, intended as a quick learning aid for engineers considering using the MAX6954 to drive 16-segment monocolor LEDs.

The MAX6954 is a versatile display driver, capable of controlling a mix of discrete, 7-segment, 14-segment, and 16-segment LED displays through a serial interface. This application note shows a typical application and configuration for driving eight mono-color, 16-segment LEDs.

See the MAX6954 data sheet for additional information about MAX6954 features.

"Quick-Start: Driving 7-Segment Displays with the MAX6954" and "Quick-Start: Driving 14-Segment Displays with the MAX6954" are similar application notes that discuss configuring the MAX6954 for 7-segment and 14-segment applications, respectively.

A common application for the MAX6954 is driving up to eight 16-segment mono-color LEDs. This application note guides the user through the process of connecting the MAX6954 to 16-segment displays and configuring the internal registers to control the displays using the included 104-character font map.

The MAX6954 utilizes a multiplex technique that reduces driver pin count by using ports alternately as cathode and anode drivers. This differs from the standard LED multiplex connection, which uses separate driver pins for anodes and cathodes. The technique is discussed in "Charlieplexing - Reduced Pin-Count LED Display Multiplexing". Table 1 lists the connection scheme for 16-segment digits that is compatible with the MAX6954 multiplex scheme and the built in 104-character font map. The letters in Table 1 correspond to the segment labels shown in Figure 2. Figure 1 illustrates an eight digit, 16-segment application circuit for the MAX6954.

Figure 1. MAX6954 16-segment application circuit.
For Larger Image

Figure 1. MAX6954 16-segment application circuit.

Figure 2. Segment labeling for 16-segment displays.
Figure 2. Segment labeling for 16-segment displays.

Table 1. Connection Scheme for Eight 16-Segment Digits
DIGIT O0 O1 O2 O3 O4 O5 O6 O7 O8 O9 O10 O11 O12 O13 O14 O15 O16 O17 O18
0 CCO   a1 a2 b c d1 d2 e f g1 g2 h i j k l m dp
1   CC1 a1 a2 b c d1 d2 e f g1 g2 h i j k l m dp
2 a1 a2 CC2   b c d1 d2 e f g1 g2 h i j k l m dp
3 a1 a2   CC3 b c d1 d2 e f g1 g2 h i j k l m dp
4 a1 a2 b c CC4   d1 d2 e f g1 g2 h i j k l m dp
5 a1 a2 b c   CC5 d1 d2 e f g1 g2 h i j k l m dp
6 a1 a2 b c d1 d2 CC6   e f g1 g2 h i j k l m dp
7 a1 a2 b c d1 d2   CC7 e f g1 g2 h i j k l m dp

Display test mode can be used to verify connections after connecting the MAX6954 to 16-segment displays. Display test mode overrides, but does not alter, all control and digit registers and turns all segments on. Enable display test mode by writing 0x01 to register 0x07. If a segment does not light in display test mode this indicates a connection problem that should be investigated. Write 0x00 to register 0x07 to exit display test mode.

After verification of the connections between the MAX6954 and the 16-segment displays the device must be configured for operation with 16-segment displays. Table 2 contains a list of the initial power-up states of important MAX6954 registers. When power is first applied to the MAX6954 the device is in shutdown mode, all digits are blanked, the 16-segment font map is selected and the device is set to scan the maximum eight digits. The default decode mode (0x01) and digit type (0x0C) register settings are correct for 16-segment applications.

Figure 3. 16-Segment display font map.
Figure 3. 16-Segment display font map.

Table 2. MAX6954 Initial Power-Up Register Status
REGISTER POWER-UP CONDITION ADDRESS
(HEX)
REGISTER DATA
D7 D6 D5 D4 D3 D2 D1 D0
Decode Mode 16-segment font enabled 0x01 1 1 1 1 1 1 1 1
Global Intensity 1/16 (minimum intensity) 0x02 X X X X 0 0 0 0
Scan Limit Display eight 16-segment digits: 0, 1, 2, 3, 4, 5, 6, 7 0x03 X X X X X 1 1 1
Control Register Shutdown enabled, blink disabled, blink speed is slow 0x04 0 0 X X 0 0 0 0
Display Test Normal operation (display test disabled) 0x07 X X X X X X X 0
Digit Type Digits 0 through 7 are 16 segment digits 0x0C 0 0 0 0 0 0 0 0
Intensity10 1/16 (min on), digits 1 and 0 0x10 0 0 0 0 0 0 0 0
Intensity32 1/16 (min on), digits 3 and 2 0x11 0 0 0 0 0 0 0 0
Intensity54 1/16 (min on), digits 5 and 4 0x12 0 0 0 0 0 0 0 0
Intensity76 1/16 (min on), digits 7 and 6 0x13 0 0 0 0 0 0 0 0
Digit 0 Blank digit, both planes 0x60 0 0 1 0 0 0 0 0
Digit 1 Blank digit, both planes 0x61 0 0 1 0 0 0 0 0
Digit 2 Blank digit, both planes 0x62 0 0 1 0 0 0 0 0
Digit 3 Blank digit, both planes 0x63 0 0 1 0 0 0 0 0
Digit 4 Blank digit, both planes 0x64 0 0 1 0 0 0 0 0
Digit 5 Blank digit, both planes 0x65 0 0 1 0 0 0 0 0
Digit 6 Blank digit, both planes 0x66 0 0 1 0 0 0 0 0
Digit 7 Blank digit, both planes 0x67 0 0 1 0 0 0 0 0

The configuration register (0x01) is used to enter and exit shutdown, control the blink function, globally clear the digit data and to select between global or digit-by-digit control of intensity. The configuration register contains 7 bits (Table 3):
  • S bit selects shutdown or normal operation (read/write).
  • B bit selects the blink rate (read/write).
  • E bit globally enables or disables the blink function (read/write).
  • T bit resets the blink timing (data is not stored-transient bit).
  • R bit globally clears the digit data for both planes P0 and P1 for ALL digits (data is not stored-transient bit).
  • I bit selects between global or digit-by-digit control of intensity (read/write).
  • P bit returns the current phase of the blink timing (read only-a write to this bit is ignored).
Table 3. Configuration Register Format
CONFIGURATION
REGISTER
DATA BIT
DATA
BIT
LABEL
STATE FUNCTION
D7 P 0 P1 Blink Phase
1 P0 Blink Phase
D6 I 0 Intensity for all digits is controlled by one setting in the Global
Intensity Register
1 Intensity for digits is controlled by the individual settings in the
Intensity10 through Intensity76 registers.
D5 R 0 Digit data for both planes P0 and P1 are unaffected
1 Digit data for both planes P0 and P1 are cleared on the rising edge of active-low CS
D4 T 0 Blink timing counters are unaffected.
1 Blink timing counters are reset on the rising edge of active-low CS.
D3 E 0 Blink function disabled
1 Blink function enabled
D2 B 0 Slow Blinking. Segments blink on for 1s, off for 1s with fOSC = 4MHz.
1 Fast Blinking. Segments blink on for 0.5s, off for 0.5s with fOSC = 4MHz.
D1 X X Don't care
D0 S 0 Shutdown
1 Normal Operation

Enable the display driver with global intensity control and without blinking by writing 0x01 to register 0x04. The internal oscillator powers as the MAX6954 exits shutdown and the oscillator output is available at OSC_OUT. Notice that the 16-segment displays remain blank, as the power-up state of digit control registers 0x60 to 0x67 is 0x20 or no segments lit (see Table 2 and Figure 3).

The MAX6954 includes a 104-character ASCII font map for 16-segment displays. The characters follow the standard ASCII font, with the addition of the following common symbols: £, €, ¥, °, µ, ±, ≠, and . Seven bits represent the 104-character font map; an 8th bit is used to select whether the decimal point (DP) is lit (Table 4). Digit registers are implemented with two planes, P0 and P1. Each digit is represented by 2 bytes of memory, 1 byte in plane P0 and the other in plane P1 (see Table 7). The digit registers are mapped so that a digit's data can be updated in plane P0 (registers 0x20 through 0x27), plane P1 (registers 0x40 through 0x47), or both planes simultaneously (registers 0x60 through 0x67). The data in the digit registers does not control the digit segments directly for 16-segment displays. Instead, the register data is used to address a character generator that stores the data for the 16-segment font (Figure 3). The lower 7 bits of the digit data (D6 to D0) select the character from the font. The most significant bit of the register data (D7) controls the DP segment of the digits; it is set to 1 to light DP, and to 0 to leave DP unlit.

Table 4. Digit Type Data Register Format
MODE ADDRESS CODE (HEX) REGISTER DATA
D7 D6 D5 D4 D3 D2 D1 D0
16-segment mode, writing digit data to use font map data with decimal place unlit 0x20 to 0x27
0x40 to 0x47
0x60 to 0x67
0 Bits D6 to D0 select font character 0 to 127
16-segment mode, writing digit data to use font map data with decimal place lit 0x20 to 0x27
0x40 to 0x47
0x60 to 0x67
1 Bits D6 to D0 select font character 0 to 127

If the blink function is disabled through the Blink Enable Bit E (Table 3) in the configuration register, then the digit register data in plane P0 is used to multiplex the display. The digit register data in P1 is not used. If the blink function is enabled, then the digit register data in both plane P0 and plane P1 are alternately used to multiplex the display. Blinking is achieved by multiplexing the LED display using data plane P0 and plane P1 on alternate phases of the blink clock.

As an example let's display eight characters, "MAXIM-IC," using the MAX6954. We disabled the blink functionality when we programmed the configuration register, so data can be written to the 0x20 through 0x27 registers to control digit 0 through digit 7, respectively. Using the font map in Figure 3 determine the code equivalent for each character:

Table 5. MAXIM-IC Example
REGISTER
ADDRESS
(HEX)
DIGIT CHARACTER FONT MAP EQUIVALENT CODE
DECIMAL HEX
0x20 0 M 0100 1101 0x4D
0x21 1 A 0100 0001 0x41
0x22 2 X 0101 1000 0x58
0x23 3 I 0100 1001 0x49
0x24 4 M 0100 1101 0x4D
0x25 5 - 0010 1101 0x2D
0x26 6 I 0100 1001 0x49
0x27 7 C 0100 0011 0x43

Adjust the intensity of the displays by writing to register 0x02, the global intensity control register. Intensity may be adjusted between 0x00 (minimum on, 1/16 current) and 0xFF (maximum on, 15/16 current). Digital control of display brightness can also be managed individually for each digit. For full details about adjusting digit intensity and other advanced features such as GPIO and key-scan, refer to the MAX6954 data sheet.

Table 6. Quick-Start Example Command Summary
REGISTER
(HEX)
COMMAND
(HEX)
FUNCTION
0x07 0x01 Enter display test mode
0x07 0x00 Exit display test mode
0x04 0x01 Exit shutdown mode, disable blinking and select global
intensity control
0x20 0x4D Write "M" to digit 0
0x21 0x41 Write "A" to digit 1
0x22 0x58 Write "X" to digit 2
0x23 0x49 Write "I" to digit 3
0x24 0x4D Write "M" to digit 4
0x25 0x2D Write "-" to digit 5
0x26 0x49 Write "I." to digit 6
0x27 0x43 Write "C" to digit 7
0x02 0xFF Set globalk intensity to full-scale

Table 7. Partial MAX6954/MAX6955 Register Address Map
REGISTER ADDRESS (COMMAND BYTE) ADDRESS
(HEX CODE)
D15 D14 D13 D12 D11 D10 D9 D8
Decode Mode R/active-low W 0 0 0 0 0 0 1 0x01
Global Intensity R/active-low W 0 0 0 0 0 1 0 0x02
Scan Limit R/active-low W 0 0 0 0 0 1 1 0x03
Configuration R/active-low W 0 0 0 0 1 0 0 0x04
Display Test R/active-low W 0 0 0 0 1 1 1 0x07
Digit Type R/active-low W 0 0 0 1 1 0 0 0x0C
Intensity 10 R/active-low W 0 0 1 0 0 0 0 0x10
Intensity 32 R/active-low W 0 0 1 0 0 0 1 0x11
Intensity 54 R/active-low W 0 0 1 0 0 1 0 0x12
Intensity 76 R/active-low W 0 0 1 0 0 1 1 0x13
Digit 0 Plane P0 R/active-low W 0 1 0 0 0 0 0 0x20
Digit 1 Plane P0 R/active-low W 0 1 0 0 0 0 1 0x21
Digit 2 Plane P0 R/active-low W 0 1 0 0 0 1 0 0x22
Digit 3 Plane P0 R/active-low W 0 1 0 0 0 1 1 0x23
Digit 4 Plane P0 R/active-low W 0 1 0 0 1 0 0 0x24
Digit 5 Plane P0 R/active-low W 0 1 0 0 1 0 1 0x25
Digit 6 Plane P0 R/active-low W 0 1 0 0 1 1 0 0x26
Digit 7 Plane P0 R/active-low W 0 1 0 0 1 1 1 0x27
Digit 0 Plane P1 R/active-low W 1 0 0 0 0 0 0 0x40
Digit 1 Plane P1 R/active-low W 1 0 0 0 0 0 1 0x41
Digit 2 Plane P1 R/active-low W 1 0 0 0 0 1 0 0x42
Digit 3 Plane P1 R/active-low W 1 0 0 0 0 1 1 0x43
Digit 4 Plane P1 R/active-low W 1 0 0 0 1 0 0 0x44
Digit 5 Plane P1 R/active-low W 1 0 0 0 1 0 1 0x45
Digit 6 Plane P1 R/active-low W 1 0 0 0 1 1 0 0x46
Digit 7 Plane P1 R/active-low W 1 0 0 0 1 1 1 0x47



Related Parts
MAX6954 4-Wire Interfaced, 2.7V to 5.5V LED Display Driver with I/O Expander and Key Scan Free Samples  
MAX6955 2-Wire Interfaced, 2.7V to 5.5V LED Display Driver with I/O Expander and Key Scan Free Samples  


Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format (225kB)  
Share
Other Channels  Email this page to an associate or friend. 



APP 3212: Jun 25, 2004
APPLICATION NOTE 3212, AN3212, AN 3212, APP3212, Appnote3212, Appnote 3212

Share



More