Maxim at a Glance
At Maxim, we invent highly integrated solutions that make technology seamless. We channel our collective expertise to stretch the limits of technology, understand your needs, and help you get to market faster.
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
Keywords: bidirectional, current sense amp, current monitor, battery, charge current, discharge current, amplifier, amplifiers, amps Related Parts
APPLICATION NOTE 1949
Bi-directional Current-Sense with Single Output
By:
Franco Contadini
Mar 25, 2003
Abstract: Battery operated devices often need to monitor both charge and discharge currents. A dual current-sense amplifier and differential amplifier are combined to produce a single output voltage that indicates magnitude and direction of battery current.
Systems such as laptop computers and other devices that have internal charge circuitry require a precise bi-directional current-sense amplifier to monitor accurately the battery's current regardless of polarity. The MAX4377 (a dual low-cost current-sense) can be used to produce a bi-directional current monitor.
Figure 1.
Output voltage OUT_ is proportional to the magnitude of the sense voltage (VRS+ - VRS-).
OUT_ is approximately zero when VRS- > VRS+.
When VRS+ > VRS-, VOUT = (GAIN)(RSENSE)(ILOAD)
where GAIN = 20 for MAX4377T.
For example, RSENSE = 100mΩ and ILOAD = 1A produce, in the case of the MAX4377T, a full-scale output of 2V. However this circuit needs a two channel ADC in order to evaluate the charge and discharge currents. Simply adding a differential amplifier such as the MAX4198 produces a circuit with a single output able to provide the information of charge or discharge current.
Figure 2.
The output VOUT will be (OUT2 - OUT1) + REF. Using a REF voltage of 2.5V we obtain an output swing from 0.5V to 4.5V (from 2.5V to 4.5V for discharge current and from 2.5V to 0.5V for charge current).
New bi-directional current-sense amplifiers such as the MAX4070, include the differential amplifier and reference on-chip.
A similar version of this article appeared in the September 2, 2002 issue of Mundo Electronico magazine.